Write Configuration Failed

Associated with: Flow runs

This attribute indicates whether ClearSCADA’s last attempt to write the Flow Run’s configuration to the Realflo controller was unsuccessful.

Configuration is written to a Realflo controller using the Write Configuration pick action.

Possible States: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R2