SCADAPack x70

Configure the Properties on the Modbus Tab

The properties described in this section only need configuring if:

  • ClearSCADA is the configuration master, and you are configuring the SCADAPack x70 device to accept communications from another SCADA master, which itself is to communicate with the SCADAPack x70 device using the Modbus protocol. (In which case the properties apply regardless of the communications protocol that ClearSCADA uses to communicate with the SCADAPack x70 device.)

With SCADAPack x70 Analog, Digital, and Counter Configuration items, you use the Modbus tab to configure the properties that enable the SCADAPack x70 device to:

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2