SCADAPack x70

Configure the Rate of Change Properties

The SCADAPack x70 tab on the Forms of SCADAPack x70 Analog Configuration items contains a Rate of Change section. Use the section to specify how the SCADAPack x70 device is to process analog data when the analog's value is rising or falling too rapidly for your requirements. When configured to do so, the device compares the current engineering value of the analog with its value over the specified time period and calculates the rate of change. It evaluates the rate of rise or fall whenever the analog's engineering value changes.

The properties in this section only apply if the analog is associated with a T_SPx70_ADV_ANALOG SCADAPack x70 logic variable (see Specify any SCADAPack x70 Logic Requirements).

The Rate of Rise and Rate of Fall fields are 'grayed out' and unavailable for use if the Period is set to 0. Such a time period disables the feature and indicates that rate of change detection is not to be performed.


Disclaimer

ClearSCADA 2017 R2