SCADAPack x70

Configure the Value Deviation Properties

The SCADAPack x70 tab on the Forms of SCADAPack x70 Analog Configuration items contains a Value Deviation section. Use the section to specify the how the SCADAPack x70 device determines whether it should generate an event for a change in the analog's current value.

The properties only apply when using a communications protocol that supports, and is configured to enable, event generation.

With physical analog inputs, you can use the Event Deviation properties to help prevent the SCADAPack x70 device from reporting insignificant fluctuations in value to ClearSCADA. This can help reduce the bandwidth usage between ClearSCADA and the device, and improve performance of historical data access (for example, Trends).


Disclaimer

ClearSCADA 2017 R2