SCADAPack x70

Configure the Device Options

Device Configuration Options section allows you to select the roles and the associated functions that the selected device type supports. You can add or remove roles for the device at any time, for example, The device is operating as a DNP3 Slave and you want it to operate as a Modbus RTU Slave as well.

Select and enable the role and functions that you require from the list. The following functions are supported:


Disclaimer

ClearSCADA 2017 R2