SCADAPack x70

Configure the SCADAPack Controls

The SCADAPack Controls of the Settings tab allows you to configure device controls settings.

At Limit Alert Processing

Selecting this option allows you to Indicate when the overrange limit value and the underrange limit value are considered to be transgressed.

When you select this option:

  • The current value needs to exceed the overrange limit value to be considered overrange.
  • The current value needs to be below the underrange limit value to be considered underrange.

When you leave this option clear:

  • The current value needs to be equal to, or more than, the overrange limit to be considered overrange.
  • The current value needs to be equal to, or below, the underrange limit value to be considered underrange.
Time Offset from UTC

Use this field to specify a the offset from Universal Coordinated Time (UTC) for local operations such as time of day control by logic applications when the SCADAPack x70 device is operating on UTC rather than local time. Default: 0 hours.

Low Voltage Alert Level

Use the Low Voltage Alarm Level field to specify the DC supply voltage below which the SCADAPack x70 device will set the ‘Local Input Power Supply Low’ system point. Default: 23 Vdc.

To generate an alarm in ClearSCADA when the SCADAPack x70 device detects a low input voltage, create a Digital input point in the ClearSCADA database for the ‘Local Input Power Supply Low’ system point.


Disclaimer

ClearSCADA 2017 R2