SCADAPack x70

Create a Device Configuration Item

Add a SCADAPack 57x Device Configuration item to the database. This item will contain the configuration that you can download to the SCADAPack 575 to configure the actual SCADAPack unit. This type of item is available from the Devices sub-branch within the SCADAPack x70 branch of the Create New menu.

When you create the Device Configuration item, you can leave most of the configuration fields at their default values. For this tutorial, the only fields that you need to change on the Device's configuration Form are as follows:

On the Settings tab:

On the DNP3 Slave tab:

Once you have configured the Device Configuration item, you can proceed to Create a Direct Outstation.


Disclaimer

ClearSCADA 2017 R2