SCADAPack x70

Define the Event Notification Delay

The fields within the Unsolicited Message Generation (Triggered Events) section of the tab apply to unsolicited messages that the outstation sends to any DNP3 master. If an outstation is to send unsolicited messages, in addition to the fields in this section, you also have to configure the properties within the Connection to Master section of the tab.

Use the field within the Unsolicited Message Generation (Triggered Events section of the DNP3 Slave tab to specify the delay time before notification of an event is sent as an unsolicited message.

Event Notification Delay

Specify the delay between the outstation detecting a ‘Send Unsolicited’ condition, and the contents of the Event Buffer being sent as an unsolicited message. This delay can reduce network bandwidth usage because it allows the first event, and any events that occur during this period, to be sent to the DNP3 Master in a single unsolicited response.

 

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

The SCADAPack x70 device will send an unsolicited message if:


Disclaimer

ClearSCADA 2017 R2