SCADAPack x70

Periodic Event Generation

Periodic Event Generation is only supported by SCADAPack x70 devices that:

So, for example, you can enable event generation on SCADAPack x70 devices with which ClearSCADA communicates using the DNP3 protocol, and for which ClearSCADA is the SCADA master.

With such devices, you can enable the feature so that the devices' analogs and/or counters support periodic generation of time-stamped point data (see Specify any Periodic Event Generation Requirements). When the feature is enabled, the SCADAPack x70 device generates events for point data at regular intervals and stores that data in its Event Buffer. This occurs in addition to the device generating and storing events for activities such as value and state changes whenever those activities occur.

If the SCADAPack x70 devices on your system are to generate and store events periodically, you should consider:

Be aware that if a SCADAPack x70 device is configured to enable unsolicited communications, the generation of time-stamped events will not trigger an unsolicited message until the configured number of Minimum Events for the relevant event Class is exceeded. The settings associated with unsolicited message generation vary per protocol.

If you find that the initial Periodic Event Generation settings result in the event buffer becoming full in the SCADAPack x70 device, either:


Disclaimer

ClearSCADA 2017 R2