SCADAPack x70

Port Function - Modbus RTU Slave

The following configuration allows the SCADAPack x70 device to connect to a Modbus RTU Master device as a Slave.

The following two sections are displayed when you select this Port Function:


Disclaimer

ClearSCADA 2017 R2