SCADAPack x70

Port Function - Terminal Server

This allows you to connect to a TCP port on a remote TCP/IP node, such as a terminal server, or another SCADAPack x70 device port that is configured as a Server port.

It can also be used to connect to an application on a host computer, or another SCADAPack x70 device port that is configured as a Client port.


Disclaimer

ClearSCADA 2017 R2