SCADAPack x70

Specify the Modbus Data Type

The Modbus tab on the Forms of SCADAPack x70 Analog, Digital, and Counter Configuration items contains a Modbus Data Type field.

Use the field to specify how the point's value is formatted in the Modbus register, and therefore the format in which the data is transmitted. The options vary, depending on the type of point:

Analog

Option Description
UINT Unsigned integer (16-bit value)
INT Integer (16-bit value)
DINT Double integer (32-bit value)
Real Real number (32-bit value)

Digital

Option Description
Discrete Boolean (bit) value

Counter

Option Description
UINT Unsigned integer (16-bit value)
UDINT Unsigned double integer (32-bit value)

Disclaimer

ClearSCADA 2017 R2