Configure the General Scanner Properties

Use the fields at the top of the Scanner tab to define the general scanner properties. Some of these fields are common to many scanners (see Define Common Scanner Properties in the ClearSCADA Guide to Simple Drivers). Those fields that are specific to scanners on the SDI-12 driver are described below.


Disclaimer

ClearSCADA 2017 R2