Minimum Configuration
This topic relates to controllers on the SE Rod Pump Controller driver.
When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:
- Those properties that require a value, but for which the property field is blank
- Those properties for which the value needs to differ from the default.
For a controller on this driver to be capable of functioning in ClearSCADA, as a minimum you have to specify these properties on the item's configuration Form:
- The outstation set with which the controller is associated (Outstation tab)
- The controller address (SE RPC tab)
- The Dynacard Stores that are to store the rod pump data (SE RPC tab)
- The Network properties for a network connected controller (Network tab)
- The Shared properties for a shared controller (Shared tab).
Also ensure that the controller and the database items on which it depends are In Service, and have saved, valid configuration. This will produce a controller that is capable of functioning using the default configuration settings.