Real Time Clock Errors
Associated with: SE Rod Pump controllers
This status attribute indicates whether the controller’s time has drifted significantly from the system time. (The maximum allowable time difference is specified on the Outstation Form (see Specify Whether ClearSCADA Sets the Controller’s Clock).)
Possible states: Displays one of the Standard Alarm States.