SE RPC Point Status Attributes

This status attribute is specific to SE RPC points:

For information about the Source status attribute that applies to Generic Advanced Modbus points that used on the SE RPC driver, see Source in the ClearSCADA Guide to the Advanced Modbus Driver.


Disclaimer

ClearSCADA 2017 R2