SE RPC Specific Status Display Attributes
This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.
Further Information
Status attributes supported by this driver's parent driver: see Advanced Modbus Specific Status Display Attributes in the ClearSCADA Guide to the Advanced Modbus Driver.