Upload Historic Dynacard

Associated with: SE Rod Pump controllers

Security permission required to access this pick action: Retrieve Data

ClearSCADA can retrieve an SE Rod Pump controller's historic dynacard data automatically, at the frequency specified on the Outstation Form (see Define the Dynacard Poll Intervals).

If required, use the Upload Historic Dynacard pick action to retrieve historic dynacard data between scheduled polls.

NOTE: If using this pick action with the Automation Interface, you need to specify the method name UploadHistoricDynacards.


Disclaimer

ClearSCADA 2017 R2