ASN Data Type

Associated with: SNMP points

The syntax used for SNMP is Abstract Syntax Notation 1 (ASN.1). The syntax defines, for example, the type of data that is accessed using the SNMP protocol. ASN.1 is used within the MIB database at each SNMP database.

The ASN Data Type attribute indicates the data type with which the point is associated.

Possible States: These vary, depending on the point type:

Every type of point:

Additionally, this Integer point is supported:

ClearSCADA does not support the data type ASN OBJECT IDENTIFIER and ASN COUNTER64.


Disclaimer

ClearSCADA 2017 R2