SNMP Specific Status Display Attributes

Every item in the ClearSCADA database has its own Status display (also referred to as a View window or View dialog). You view an item's Status display by selecting that item's View Status pick action or menu option. The Status display provides information about the status of the selected item, presenting the information in the form of 'status attributes'. For further information about working with Status displays, see Status Displays.

Example:

The Status display for an SNMP device or point provides information about the present state of that device or point.

The database items that are associated with this stand-alone driver support a combination of:


Disclaimer

ClearSCADA 2017 R2