Export SQL Query Result

Associated with: SQL Exports

Security permission required to access this pick action: Control

If the data is being exported to removable media, please check that the media is at the required location and is available for use. For example, if the data is to be stored on a CD-R, a suitable CD-R needs to be inserted in the CD-RW driver of the server before the SQL query result is exported.

Use this pick action to execute the SQL Query that is associated with an SQL Export item and export the result of that query. The location to which ClearSCADA exports the result and the format that the output file takes is pre-defined, using fields on the SQL Export Form (see Add and Configure an SQL Export).

If you are using this pick action with the Automation Interface, you need to specify the method name Export. (Refer to the Database Schema for argument naming conventions used with the Automation Interface.)


Disclaimer

ClearSCADA 2017 R2