Specify a Trip Sequence for a Date

To specify a trip sequence for a date, you enter the trip code:

%D<format>%

where <format> is one or more of the Windows® picture string date formats that ClearSCADA supports (see Supported Trip Codes for Dates).

To specify the date that ClearSCADA substitutes for the trip code, you use the Trip Sequence Time field on the SQL Export Form’s SQL Export tab.

The default of NOW results in a time of ‘now’ exactly. If an offset time stamp is required, you can specify another time value in the OPC Relative Time Format.

For an example of how to use the Trip Sequence Time in conjunction with the trip sequences that you can specify for an SQL Export item’s Output File Name, see Specify the Trip Sequence Time.

Further Information

Resolving any Trip Sequence Errors.


Disclaimer

ClearSCADA 2017 R2