Join Order

A join order is a permutation of the order in which the tables referenced in your query are searched.

Example:

If your query is being used to search two tables - Table A and Table B, the possible join orders are:

  • A, B
  • B, A

The order in which the tables are searched can have a significant effect on the performance of a query. For this reason, the Query Processor calculates the Cost for each Access Plan, and then uses the results to determine which joint order is the most efficient.


Disclaimer

ClearSCADA 2017 R2