You can disable the execution of global and mimic scripts if one or more scripts prevent a ViewX client from launching or functioning correctly.
To disable the execution of global and mimic scripts you need to launch ViewX using the /noscript ViewX command.
To use the /noscript argument:
- In Microsoft Windows, run the Command Prompt.
- When the prompt is displayed, use the change directory command to locate your ViewX application.
                For example, if your command prompt shows Documents and Settings\<Your Windows ID> when you first display it, you need to enter: cd <the location of your ViewX application> Do not include the angle brackets. For example: cd C:\Program Files\Schneider Electric\ClearSCADA 
- Press the Enter key. The command prompt should change to show the location of your ViewX application.
- When the prompt shows the location of your ViewX application, enter: SE.Scada.ViewX.exe /noscript 
- Press the Enter key. 
 ClearSCADA will disable all global and mimic scripts and launch ViewX.Alternatively, you can enter the location of your ViewX application and add the suffix of SE.Scada.ViewX.exe /noscriptas the Target of a desktop shortcut. You can then use the desktop shortcut to run the /noscript command. There has to be a space betweenSE.Scada.ViewX.exeand/noscript. For more information on desktop shortcuts, please refer to the documentation supplied with your Windows operating system.