RadioButton.Checked
The RadioButton Control Object that is returned by the AddRadioButton function has a Checked property. The Checked property defines whether the Radio Button is selected.
| Syntax |
ControlObject.Checked = Value Where ControlObject. is the name of the variable (declared in your script) that is used to store the RadioButton Control Object that is returned by the AddRadioButton function. |
| Description |
Sets the RadioButton to be selected or de-selected. |
| Arguments |
Value {Boolean} If set to True (1), the Radio Button is selected automatically by default; if set to False (0) it is de-selected. |
| Returns |
Boolean |
Example:
RadioButton1.Checked = 1
Where:
- RadioButton1 is the name of the variable that stores the RadioButton Control Object returned by the AddRadioButton function
- 1 sets the Radio Button to be selected.