Server.RootObject
The RootObject property is a server property that represents the top level item in the database.
Syntax |
Server.RootObject |
Description |
Represents the top level of the database (the Root of the database). |
Arguments |
None. |
Returns |
ServerObject A ServerObject is a ClearSCADA specific script object that has its own functions (see ServerObject Functions ) and properties (see ServerObject Properties) which can be manipulated. |
Example:
The following script is used to display a message box that contains the name of the root object:
Set ServerRoot = Server.RootObject
MsgBox ServerRoot.Name
Where:
- ServerRoot is the name of the variable used to store the ServerObject that is returned by the RootObject property.
- MsgBox ServerRoot.Name instructs the script to display a message box that contains the Name value of the ServerObject that is stored by the ServerRoot variable (this is the ServerObject that is returned by the RootObject property).