User Messaging Functions
ClearSCADA includes an in-built user messaging system that allows users to send messages to other logged on users. By default, these messages are processed by ClearSCADA and are displayed in standard message dialog boxes on the recipients’ clients. However, by using the user messaging function and VB Script, you can define different functionality that will occur when a client receives a user message.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.