X and Y

The X Control Object property allows the script to set the X-Axis coordinate of the Control Object, and the Y Control Object property allows it to set the Y-Axis coordinate.

Syntax

ControlObject.X = Number or ControlObject.Y = Number

Where ControlObject is the name of the control object that you are positioning and Number is the number for the coordinate.

Description

Sets the position of the Control Object on the X-Axis (horizontal positioning) or Y-Axis (vertical positioning)

Arguments

ControlObject {string}

The name of the Control Object that you want to position.

 

Number {integer}

The number for the X-Axis or Y-Axis coordinate.

Returns

Integer.

Example:

AlarmButton.X = 10

This would position the control named AlarmButton at X coordinate 10.


Disclaimer

ClearSCADA 2017 R2