Define the Certificates Settings for Original WebX Clients

This section and associated topics primarily apply to the Original WebX client only. However, if you are using Mimics in WebX, you still need to configure the Certificates for Original WebX.

To help protect your system against unauthorized access, ClearSCADA uses certificates for Original WebX clients.

The certificates allow the ClearSCADA server to use encryption for client-server communications.

There are two types of certificate that ClearSCADA can use for Original WebX:

If a server generated non-trusted SSL certificate is used, the client will display warning messages when users access the system. The exact warning message depends on the browsers, but typically might be "There is a problem with this website’s security certificate". Some users may find these warning messages distracting, although they do not affect their ability to interact with your ClearSCADA system.

If a trusted SSL certificate is used, the client is able to verify that it is connecting to the expected server, and so there are no warning messages shown when a client accesses the secure web server ports.

We recommend that you purchase trusted SSL certificates for your web servers so that users do not receive distracting warning messages. We also recommend you review your security options and establish appropriate security for your web server.

Recommended security:

Maximum security:

Not recommended:


Disclaimer

ClearSCADA 2017 R2