Recommended Security Settings

When you first install ClearSCADA, the Security feature is enabled by default. The default values for the various security-related settings are intentionally set at a high level. Initially you use the Super User account to access the server configuration features. This is so that an administrator can gain access to the many features that are needed during the setting up of a system.

To help protect your system against unauthorized users and also from accidental changes made by inexperienced users, you should configure the security settings to meet your own requirements.

While each system and organization is different, there are some common actions you can take to improve the security of your system. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2