Take Complete Exclusive Control

Associated with: Every database item

Security permission required to access this pick action: Manage Exclusive Control.

The Take Complete Exclusive Control action allows you to take exclusive control of an item or a group of items. When you take exclusive control of an item, other users cannot access the reserved features for the item (until the exclusive control is released, either by you or by another user with the Manage Exclusive Control permission).

Take Complete Exclusive Control is available on an item’s context sensitive menu when all of the following conditions are true:

If the item for which you want to take complete exclusive control is a Group, the Take Complete Exclusive Control action is only available if all of the conditions above are true and all of the items in the Group are either under your exclusive control or not under exclusive control at all. If any of the items in the Group are under the exclusive control of another user, the Take Partial Exclusive Control action is made available instead of the Take Complete Exclusive Control action.

Further Information

Taking Exclusive Control

Take Partial Exclusive Control.


Disclaimer

ClearSCADA 2017 R2