Use DMZ Servers instead of Permanent Standby Servers
If your system architecture has permanent standby servers that are only used to read data from ClearSCADA, you can improve your security by reconfiguring them as De-Militarized Zone servers (DMZ servers).
DMZ servers can run outside a firewall and have a single, read-only connection to ClearSCADA. The read only connection means that it is impossible for the ClearSCADA software on the DMZ server to write to the ClearSCADA database.
However, vulnerabilities in the operating system that runs on the DMZ server can potentially expose your system to unauthorized access. To avoid this, you can use your DMZ server outside a firewall—the firewall can be set to help protect your system against unauthorized access via the operating system.
The table below shows the benefits of using a DMZ server outside a firewall in comparison to a DMZ server without a firewall or a read-only permanent standby server.
ClearSCADA software can read from ClearSCADA database | ClearSCADA software can write to ClearSCADA database | Protection against misuse of ClearSCADA software on Server |
Protection against Operating System Vulnerabilities |
|
---|---|---|---|---|
Permanent Standby Server (used as a Read Only server) |
Yes |
Yes |
ClearSCADA user accounts Windows user accounts |
No |
DMZ Server |
Yes |
No |
ClearSCADA on DMZ server cannot write to the ClearSCADA database. ClearSCADA user accounts Windows user accounts |
No |
DMZ Server
|
Yes |
No |
ClearSCADA on DMZ server cannot write to the ClearSCADA database. ClearSCADA user accounts Windows user accounts |
Yes. Firewall can be set to help protect against non-ClearSCADA vulnerabilities. |
For maximum security, we recommend that instead of read-only servers, you use DMZ servers that run outside a firewall.
If your requirements mean it is impractical to use a firewall, we still recommend that you use a DMZ server instead of a read-only server. Using DMZ servers means you have the added protection of the single, read-only connection between the ClearSCADA software on the DMZ servers and the ClearSCADA database.
Even without a firewall, a DMZ server offers greater protection than a permanent standby server as it has no write connection to ClearSCADA.
To configure a server as a DMZ server, see De-Militarized Zone (DMZ) Permanent Standby Servers.