Use Secure Web Ports with a Trusted SSL Certificate

Your ClearSCADA system can be accessed via the Internet or a company Intranet. To provide this functionality, ClearSCADA uses web ports for both the legacy ClearSCADA web server and for the IIS web server. The latter configuration is managed using the Windows IIS settings tool. Please consult Windows help for assistance in setting up IIS securely.

There are two sets of web ports:

When a web browser accesses a web server via the secure sockets protocol (https), the web browser will request the server's SSL certificate. The web browser uses the information in the certificate to:

If an administrative user has not already configured an SSL certificate in the web server, ClearSCADA will automatically create a top-level non-trusted SSL certificate for that web server.

If the default, server generated non-trusted SSL certificate is used, the WebX client will display warning messages when users access the system. The exact warning message depends on the browsers, but typically might be "There is a problem with this website’s security certificate". Some users may find these warning messages distracting, although they do not affect their ability to interact with your ClearSCADA system.

If a trusted SSL certificate is used, the WebX client is able to verify that it is connecting to the expected server, and so there are no warning messages shown when a WebX client accesses the secure web server ports.

We recommend that you purchase trusted SSL certificates for your web servers as this will mean that users do not receive distracting warning messages. We also recommend you review your security options and establish appropriate security for your web server.

Recommended security:

Maximum security:

We recommend that you do not :

For more information, see Setting Up Security for WebX and Original WebX Clients.


Disclaimer

ClearSCADA 2017 R2