Communications Logging Status on Mimics

Mimics can contain animated representations of a channel. The Mimic can be configured to indicate the channel's log status as a background color. If logging is enabled on the channel, the background is dark yellow/mustard (default settings).

If logging is disabled on the channel, the background color is white (default settings).

The change of color is a visual indication of logging being enabled. This can act as a reminder that logging needs to be disabled (it should only be enabled when you need to monitor communications).

To access a Mimic that contains an animated representation of a channel, you can:

Either:

  1. Use the Database Bar to locate the Mimic.
  2. Right-click on the Mimic's entry.
    A context-sensitive menu is displayed.
  3. Select the Display Mimic option.
    The Mimic is displayed.

Or:


Disclaimer

ClearSCADA 2017 R2