Configuration Change CRC Server Setting

The Global Parameters branch of the Server Configuration Tool includes an Advanced section.

Use the Configuration Change CRC setting in the Advanced section to determine whether Configuration Change CRC values are exposed via ViewX and WebX clients. The CRC values can be used to help to determine whether configuration changes have been made to the database since the CRC values were last read and recorded. For information on using CRC values, see Understand Configuration Change CRCs in the ClearSCADA Guide to the Database.

Further Information

Use the Configuration Change CRC check box: see Enable or Disable the Configuration Change CRC Feature in the ClearSCADA Guide to the Database.


Disclaimer

ClearSCADA 2017 R2