Define the Data Section for a Standard Custom Field

If you are adding or modifying a Standard type of custom field, you can use the Section setting to define the data section in which the field will be stored.

ATTENTION: Your choice of data section can affect system performance, so you need to choose an appropriate setting.

To define the data section for an extra field, you need to use the Edit Field window (see Add or Modify an Extra Field).

When you have displayed the Edit Field window, you can define the data section by using the Section setting:


Disclaimer

ClearSCADA 2017 R2