Define the Number of Characters Permitted in an Extra Field

If you are adding or modifying a Standard type of custom field or a Search Key type of custom field, you can use the Size setting to define the number of characters that are permitted for the field. With Search Key fields, the Size setting determines the number of characters that are included when data is returned via ODBC.

To define the number of characters permitted in an extra field, you need to use the Edit Field window (see Add or Modify an Extra Field).

When you have displayed the Edit Field window, you can define the number of permitted characters by using the Size setting:

When you have defined the Size, you can continue to define the other field settings as required.


Disclaimer

ClearSCADA 2017 R2