Driver Logging
Each driver can generate log files that contain information about the driver's activity. These log files can then be used to diagnose unexpected driver behavior.
To setup driver logging, you need to Define the Driver Logging Settings. When you have setup the driver logging, you can use the ClearSCADA Server Status Tool to Display a Driver Log File.
You can also use a Telnet client to monitor a driver in real time (see Telnet Monitoring).