Example Configuration: Database Backup
You can configure ClearSCADA to back up your database at regular intervals. You might also want to consider the following:
- You can configure a Schedule to back up the database automatically at regular intervals. For example, every week
- You can create a Mimic that shows the progress of the backup
- If you want to send a backup to a remote computer over a slow network, you might want to back up your ClearSCADA database locally first, then zip up the backup files and copy the zip file to the remote server.
The topics in this section comprise various examples to show how you might configure the backup feature in ClearSCADA. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.