Memory Requirements for Citrix XenApp and Microsoft Remote Desktop Services

(Microsoft Remote Desktop Services was formerly known as Microsoft Terminal Services.)

Each Citrix server or Remote Desktop Services server requires an appropriate amount of memory and disk space to run:

Each ViewX session requires the same amount of RAM and hard disk space as a ViewX client:

For example, if you require 8 Citrix or Remote Desktop Services clients, the Citrix/Remote Desktop Services server needs:

plus

For information on the minimum specifications for Citrix XenApp, Microsoft Remote Desktop Services, the server operating systems and any other applications, please refer to the manufacturer’s documentation.


Disclaimer

ClearSCADA 2017 R2