Remove a Historic View

You can remove any Historic Views that are no longer needed. But before you delete a Historic View, you should first check that the Historic View is not needed by internal or external applications.

To remove a Historic View:

  1. Access the ClearSCADA Server Configuration Tool (see Run the Server Status Tool).
  2. Expand the SQL Query Configuration branch.
  3. Select Historic Views.
  4. Right-click on the Historic View that you want to edit from the list of historic views, and then select the Delete option.
  5. Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.

Now that you have deleted a historic view, you can either proceed to configure other Historic settings (see Historic Configuration Settings) or you can continue with the server configuration.

If you are unfamiliar with the server configuration process, we recommend that you proceed to learn about Point State Alarms.


Disclaimer

ClearSCADA 2017 R2