Using a Registry Editor to Change Server Log File Settings
You can use a registry editor such as Regedit to make changes to the log file settings (such as maximum number of files, location of files, and so on). For some applications, such as port server, the only way to alter the log file settings is to use a registry editor.
To use a registry editor to change log file settings:
- Select the Start button on the Windows taskbar, and then select the Run option to display the Run window.
(On a machine using an operating system such as Windows 7, you will need to select the All Programs option, followed by Accessories, and then select the Run entry.)
- Enter the following text in the Open field and select OK to run the registry editor:
Regedit
- Use the Registry Editor to locate the registry settings at the relevant location.
The default locations are as follows:
Alarm and Events Printer
On 32-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\AEPrinter
On 64-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ClearSCADA\AEPrinter
Drivers
The registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\Driver<Driver Name>
For example:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\DriverSCADAPackModbus
Channels
Communications logs use the same settings as the relevant driver (see Locating the Log Files). There are no registry settings for channel logs.
License Server
On 32-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\LicenseServer
On 64-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ClearSCADA\LicenseServer
Port Server
On 32-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\PortServer
On 64-bit systems, the registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\ClearSCADA\PortServer
Server
The registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\DB
Rather than use a registry editor to change the Server log file settings, you can use the Server Configuration Tool (see Define the Server Logging Settings).
Server Snapshot
The registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\DBSnapshot
Additionally, several other registry settings are at:
HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\ClearSCADA\DB
These are:
ResetCountersOnSnapshotEnter True, Yes, T, Y, or 1 to reset the accumulative counters after each server snapshot is logged, or enter False, No, F, N, or 0 to disable resetting of the accumulative counters, as required. The default is False.
SnapshotEnableEnter True, Yes, T, Y, or 1 to enable server snapshot logging or enter False, No, F, N, or 0 to disable server snapshot logging as required. We recommend that you enable the logging unless requested to do otherwise by Schneider Electric.
SnapshotIntervalSpecify the frequency (in minutes) at which server snapshots are taken. The minimum value that you can enter is 1 minute; the maximum value is 1440 minutes (1 day). If you schedule server snapshots to occur more than once a day, we recommend that you specify an interval that is a divisor of 60, so that the snapshots occur at the same time each day. The default is 30 minutes.
For ViewX logging, ODBC Logging, and DB Client Logging, see Using a Registry Editor to Change Client Log File Settings.
- Define the registry settings:
- Right-click on a setting to display a context sensitive menu. The settings include:
LogEnable
Enter True, Yes, T, Y, or 1 to enable logging or enter False, No, F, N, or 0 to disable logging as required.
LogFileBaseDefine the folder that will contain the log files and the filename prefix for the files. The prefix is the name of the files (it cannot contain certain characters, see your operating system documentation for more details).
LogMaxFilesEnter the maximum amount of log files permitted for each set of log files. When a new log file is created, the oldest log file is deleted (to make way for the new file).
LogMaxSizeEnter the largest possible size for a log file. The size is in kilobytes.
LogOldFilesEnter the number of sets of log files that can be stored for each instance of an application.
For many systems, the default setting of 1 is adequate.
LogTelnetPortEnter the port number for the Telnet server (enter 0 if the port is to be assigned dynamically or enter the specific number of the port as required). The LogTelnetPort is only available for those applications that contain a Telnet server (see Telnet Monitoring).
- Select the Modify option to display the Edit window.
- Enter the required setting in the Value Data field (see step i for the required settings).
- Select the OK button to confirm the setting.
- Repeat the sub-procedure (i-iv) for each logging setting.
- Right-click on a setting to display a context sensitive menu. The settings include: