What is a Good Setup for a System that has an Unreliable Network Connection?

We recommend that you only use reliable connections between the Main and Standby servers. However, if this is not possible, you can use the Duty Mode feature (Duty Duty) to restrict the effect that intermittent connections can have on the system. This is dependent on the type of outstations and PLCs being used (they have to be able to connect to either of the servers independently).

For more information, see Enable or Disable Duty Mode.


Disclaimer

ClearSCADA 2017 R2