Buffers

ClearSCADA uses internal buffers to help ensure that sufficient memory is available for performing critical tasks. The internal buffers are blocks of memory that are permanently allocated for use with frequent tasks.

Status information about the internal buffers is shown in the Buffers category on the Server Status Tool. Typically, this information is only used by Schneider Electric engineers when investigating potential memory issues on systems with large databases.

The buffers status information is categorized as:


Disclaimer

ClearSCADA 2017 R2