ConfigChanges Searches

The ConfigChanges Searches category contains information about the searches that are currently requesting data from the Configuration Changes Auditing files. You can use the information to determine if a slow response to a Configuration Changes request is due to a large search or another factor such as abnormal network conditions.

The ConfigChanges Searches category displays the following information:


Disclaimer

ClearSCADA 2017 R2