Information
The Information category provides status information about the current status of the server's hardware and software.
The Information category provides a variety of information about the server, including:
- The version of ClearSCADA that is running on the named server
- The current state of the server, for example, Main
- The time that the server changed to its current state
- The time that the server last became Main
- The amount of available memory on the server
- The amount of available paging file
- The operating system that is being used
- The server ports that are in use and the applications that are using them, for example, the WebX server
- The number of ViewX clients and WebX clients that are connected to the server.