Reference Field Indices

Many reference fields in the ClearSCADA database are indexed. The indices are used internally to provide a record of the references between database items (such as the references between Group Instances and their Group Templates). Indices also allow for faster queries of indexed fields, as the query can be performed on an index rather than the entire database.

The Reference Field Indices category on the Server Status Tool shows which fields are indexed, and provides information about the number of target and source fields and the names of each index.

The information in the Reference Field Indices category can be useful when investigating the cause of queries that are performing slower than expected—the slower return time may be due to the query being performed on reference fields that are not indexed.

The status information is categorized as:


Disclaimer

ClearSCADA 2017 R2