Threads

The Threads category provides status information about the threads that are in use by the server. Each thread is a separate execution path within a process. For example, the DB Event thread is an execution path within the ClearSCADA Database Server process. The threads allow the process to perform multiple tasks simultaneously.

The status of each thread is categorized as:


Disclaimer

ClearSCADA 2017 R2