Transactions

ClearSCADA uses configuration transactions to allow certain operations, such as Group Instance propagation, to run in the background. Users can continue to work with various other features while the background operations take place.

The operations that use transactions are:

When an operation that uses transactions is actioned, the transaction is added to the configuration transaction queue. ClearSCADA performs the transactions in the queue in turn, over short periods. These periods are calculated internally by ClearSCADA to provide sufficient resources and so cannot be adjusted manually.

At the end of each period, ClearSCADA stops performing the transactions so that other operations such as driver updates can take place. Upon resuming the transactions, ClearSCADA continues from the previous position in the configuration transaction queue.

You can use the Transactions section on the Server Status Tool to view the current transactions:

The status information is categorized as:


Disclaimer

ClearSCADA 2017 R2