XML-DA Items

The XML-DA Items category provides status information about the XML-DA tags to which XML-DA clients are subscribed. Status information is shown for XML-DA tags when XML-DA is used to access the database. Each XML-DA tag represents a path to a value for an item.

The status information for each XML-DA tag is categorized as:


Disclaimer

ClearSCADA 2017 R2